IMTS 2026 News Hub
Check out the latest products and innovations
Interested in what's to come at the show? See below for all the latest news and updates on Renishaw's involvement at IMTS. Discover cutting-edge technology and the latest advancements in manufacturing.
Book a consultation with a sales representative

RMP400S: All-in-one machine tool probing solution
Renishaw is pleased to announce the market introduction of its multi-purpose RMP400S. The RMP400S an innovative solution that seamlessly combines touch-trigger, scanning, and surface finish verification into a single machine tool probe. This powerful combination makes it Renishaw's most versatile spindle probe to date, delivering exceptional metrology performance. Read more >>

RUP60: Ultrasonic thickness measurement probe
Renishaw will unveil its new advanced ultrasonic thickness measurement probe, the RUP60, in Chicago at IMTS 2026. This new probe simplifies the measurement of large parts where access is limited to a single side, removing the need to move parts to specialist measurement equipment or perform manual inspection on the machine. Read more >>
Introducing Equator-X™ dual-method gauging system
Two systems in one: the Equator-X gauging system delivers exceptionally fast production-CMM performance and comparator gauging. The dual-method capability offers the flexibility to quickly validate first-off components or perform 100% inspection of parts up to 500 mm in diameter. Users can select the inspection method that best suits your manufacturing process. Download brochure >>

New, powerful MODUS™ IM Equator software
This new software enables customers to assign simple measurement features easily with a user-friendly CAD interface, and with no code required. It automatically ensures all machine movements are collision-free, and all settings follow metrology best practice. These features enable users to quickly address new part requirements and ensure high uptime for production lines. Read more >>