Machine tools - precision encoders for accurate machining

Vital to modern manufacturing, machine tools allow you to achieve complex component production with high levels of accuracy, efficiency and repeatability. Applications include milling, turning, grinding, electrical discharge machining (EDM), laser cutting, and 3D printing.

The vital role of encoders in machining


Renishaw's optical and magnetic encoder products.jpg

Why use encoders in precision machining?


Accurate positioning and motion control are essential for precision manufacturing. Parts produced on machines with unreliable position feedback can result in costly errors, material waste and low productivity. Encoder technologies ensure the accuracy, reliability and performance of machines where motion control is critical.

Illustration of a 5-axis CNC milling machine, explaining the role of encoders in linear, spindle, and rotary motions controls..jpg
Picture of a 5-axis CNC milling machine.jpg
Motion control in a 5-axis CNC milling machine: linear, spindle, and rotary movements. 


Linear axis encoders


What is a linear axis in CNC machining?


In CNC precision machining, a linear axis refers to the straight-line movement of a machine tool, typically along the X, Y, and Z axes. 

These three linear axes enable precise positioning and motion control in three-dimensional space, which is essential for accurate tool and workpiece alignment. High-precision movement directly impacts dimensional accuracy, surface finish, and overall part quality.


What are linear encoders and why do they matter?


Enclosed linear encoders are designed to deliver reliable performance even in harsh machine tool environments, including exposure to vibration, lubricants, and temperature fluctuations.

➤ Key benefits of linear encoders


  • Position feedback - Linear encoders provide accurate and real-time feedback on the position of the linear axis. This information is essential for the CNC controller to ensure that the tool or workpiece is precisely positioned according to the programmed instructions.
  • Closed-loop control - The CNC system utilizes closed-loop control, where the feedback from the linear encoder is continuously compared with the commanded position. Any discrepancies trigger adjustments to the motor movements, ensuring that the actual position matches the desired position.
  • Precision machining - The high resolution of linear encoders enables CNC machines to achieve fine positional increments, leading to precise machining operations. This is crucial for producing accurate and high-quality parts.

A 5-axis CNC with Fortis enclosed encoder installed.gif
A CNC milling machine with Renishaw’s FORTiS™ enclosed encoder installed on its linear axes

Why choose Renishaw’s FORTiS™ encoder for linear axes?


Renishaw's FORTiS™ linear encoder features a sealed design that protects against contamination from fluids and debris, making it ideal for demanding machine tool applications.

It supports fine positional increments, enabling high-resolution machining and improved productivity.
Fortis_linear_axis_on_CNC.jpg
Real-world example: HEAKE Precision has selected the Renishaw FORTiS enclosed linear encoder for its latest machining centres to provide direct position feedback.



Spindle axis encoders


What is a spindle axis in CNC machining?


The spindle axis is an essential component in machine tools, driving the rotation of cutting tools or workpieces. As the core of the machine's rotational drive system, it enables operations such as turning, milling, and drilling.

Typically, the spindle axis functions at high speeds and with high precision. The stability of its rotational speed and the accuracy of its angular control are critical factors that directly influence the quality and efficiency of machining processes.

What are spindle encoders and why do they matter?


These dynamic settings demand exact synchronisation of angle control, speed, and feed rate – think of typical applications like CNC automatic tool changers (ATC) and thread tapping process, where timing and accuracy are paramount.

Just like linear encoders, spindle encoders must operate reliably in harsh industrial environments—withstanding vibration, coolant exposure, and thermal fluctuations.

Spindle of a 5-axis CNC milling machine.jpg
Spindle axis of a CNC machine.jpg

➤ Key benefits of spindle encoders


  • Speed control - Spindle encoders provide feedback on the rotational speed of the spindle. This information is crucial for maintaining the desired cutting speeds during machining processes. It allows the CNC controller to adjust the spindle speed in real-time to match the programmed parameters.
  • Tool synchronization - In multi-tool machining or tool changes, spindle encoders help synchronize the movements of the spindle with the tool change process. This ensures smooth transitions and prevents collisions between the tool and the workpiece.
  • Thermal compensation - Spindle encoders contribute to thermal compensation by providing feedback on temperature-related changes in the spindle. This information allows the CNC system to adjust the machining parameters to account for thermal expansion or contraction.

Why choose Renishaw’s SpinCo™ encoder for the spindle axis?


SpinCo™ incremental magnetic encoder system is purpose-built for spindle applications. It utilises advanced AMR and GMR sensor technologies to deliver high-resolution feedback, even under extreme operating conditions typical of CNC machining.

SpinCo's automatic gain control (AGC) ensures consistent signal quality, while the integrated LED status indicator simplifies installation and diagnostics.


Rotary axis encoders


What is a rotary axis in CNC machining?


A rotary axis in CNC machining enables rotational movement of the tool or workpiece around a fixed point. Unlike traditional linear axes (X, Y, Z), rotary axes add angular motion, allowing for multi-axis machining, complex geometries, and greater precision.

What are rotary encoders and why do they matter?


Rotary axes are commonly found in 4-axis and 5-axis CNC machines, where they enhance flexibility and reduce the need for multiple setups. This leads to faster production times and improved surface finishes.

Direct–drive (DD) rotary tables are commonly employed to boost production efficiency by the precision machining industry. To guarantee accuracy, open-type encoders are often used as they do not require mechanical coupling between the scale and the encoder.

Rotary table in a CNC machine that rotates along the rotary axis.gif
Rotary axis movement of a rotary table in a CNC machine

➤ Key benefits of rotary encoders


  • Angular position feedback - Rotary table encoders provide feedback on the angular position of the rotary table. This information is critical for applications where workpieces need to be rotated to specific angles during machining operations.
  • Indexing and contouring - CNC machines often use rotary tables for indexing or continuous contouring. The feedback from rotary encoders ensures precise angular positioning, enabling the CNC controller to execute complex machining paths and contours.
  • Multi-axis coordination - In machines with multiple axes, rotary table encoders contribute to the coordination of movements. The CNC controller uses the feedback from the rotary encoder to synchronize the rotational movements of the table with other linear and rotary axes.

A shop floor worker in Haozhi fitting an Renishaw's RESOLUTE true-absolute encoder onto a direct-drive motor.jpg
Haozhi’s direct-drive rotary tables are fitted with RESOLUTE true-absolute encoder.jpg
Haozhi’s direct-drive rotary tables are fitted with RESOLUTE series absolute encoders to enhance motion control accuracy

Why choose Renishaw’s RESOLUTE™ encoder for rotary tables?


The RESOLUTE™ absolute encoder measures position with fine resolutions down to 1 nm and high speeds up to 100 m/s, delivering high-resolution feedback for rotary tables, enabling precise angular positioning.

Real-world example: Taiwan’s Industrial Technology Research Institute developed a dual-axis rotary table using Renishaw’s RESOLUTE™ encoder. The system achieved ±10 arc seconds accuracy, ±5 arc seconds repeatability, and 0.001° angular resolution.

Not sure which encoder suits you?


How to ensure high precision in industrial environments?


In precision manufacturing, machine tools must operate reliably under a range of harsh industrial conditions that directly impact performance and accuracy.

➤ Factors that affect machining accuracy


  • Extreme temperature operation - High or low temperatures can cause material expansion or contraction, affecting both stability and precision.
  • Intense shock and vibration - Machine tools are subject to external forces during operation, which can lead to deviations in accuracy and compromise machining quality.
  • Dust and liquids - Industrial environments often contain dust, fluids, or other contaminants that can infiltrate equipment and disrupt stable operation.
  • Corrosive substances - Coolants, lubricants, and chemicals may damage internal components, reducing long-term reliability.
  • Continuous operation - Industrial machinery is expected to run for extended periods without interruption, demanding exceptional durability and stability.

➤ Durable encoder solutions for CNC machines and demanding conditions


These demanding conditions require industrial equipment to be designed and manufactured with outstanding durability, reliability, and precision.

For precision tools such as CNC machines, the choice of encoder is critical, as it directly affects motion control and positioning accuracy.
CNC_milling process.jpg

Renishaw’s enclosed linear encoders, spindle encoders, and rotary encoders are engineered to perform reliably in these challenging environments. They are designed to resist temperature fluctuations, vibration, and contamination, while maintaining high performance under extreme conditions.



What to consider when selecting encoder systems for machine tools?


The table below outlines the key factors typically evaluated when choosing an encoder system for machine tool applications. These factors include encoder performance, environment conditions, installation requirements, and other relevant considerations.

Machine tools

Performance

✔ Scale accuracy
✔ Scale linearity
✔ Resolution
✔ Sub-divisional error
✔ Scale CTE
✔ Repeatability
✔ Speed
✔ Controller input frequency
✔ Cable flex Radius
✔ Cable flex life


Environment

✔  Temperature
✔  Humidity
✔  Vibration resistance
✔  Electromagnetic compatibility (EMC)
✔  IP rating
✔ Dirt immunity
✔ Shock resistance
✔ Air purge

Installation

✔ Size
✔ Top or side mount
✔ Ride height tolerance
✔ Readhead travel orientation
✔ Cable exit direction
✔ Connectors
✔ Substrate type
✔ Mounting method
✔ Reference datum
✔ Limits


Others

✔ Analogue / digital
✔ Functional safety
✔ Alarm type
✔ Reference limit
✔ Termination
✔ Protocol


Encoder success stories: Machine tools

Heading 1

Lorem Ipsum is simply dummy text of the printing and typesetting industry. Lorem Ipsum has been the industry's standard dummy text ever since the 1500s, when an unknown printer took a galley of type and scrambled it to make a type specimen book.

Form Heading

Enhancing stability in manufacturing high-quality products

Image

Enhancing stability in manufacturing high-quality products


Machine tool accuracy is affected by a variety of environmental and physical factors including the thermal expansion of components, defects in the guide rails and bearings, and other geometric errors that occur during manufacturing.

Heake_FORTiS_encoder.jpg
Two ways of improving machine tool accuracy are: optimising the assembly process and compensating for thermal errors; and using high-performance position feedback and motion control.

HEAKE Precision Technology Company has selected the Renishaw FORTiS enclosed linear encoder for its latest machining centres to provide direct position feedback from the linear axes.

Open quotation mark

FORTiS encoders are also very easy to install. By viewing the setup LEDs, it only takes us an average of seven minutes to install the encoder on each axis.

Taking the HEAKE LH800 model as an example, the total installation time for the three axes is less than half an hour, which is twice as fast as the time taken with other encoder brands that were tried in the past.

HEAKE Precision Technology Company (Taiwan) Close quotation mark


Accelerate the performance of direct-drive motors

Haozhi is an industry leader in direct-drive technology for machine tool and robotics applications in China.

Encoders are one of the most critical components in Haozhi’s motion control products. Important encoder errors for rotary motors include sub-divisional error (SDE), jitter, installation error (which includes scale eccentricity), scale graduation error and the compliance of the coupling between the motor and the encoder rotary scale.

Open quotation mark

The LA11 was ideal because it minimised our space requirements by producing both absolute and incremental signals from one readhead and scale tape.

RESOLUTE™ encoders support most mainstream industrial comms protocols including FANUC, Mitsubishi, Siemens DRIVE-CLiQ and BiSS®. 

Haozhi Mechanical and Electrical (China) Close quotation mark

Breakthrough in multi-axis rotary table design

As multi-axis machine tool technology matures, demand for rotary tables with enhanced accuracy and rotational speed is rising.

Taiwan's Industrial Technology Research Institute (ITRI) has addressed this market trend by developing an advanced dual-axis rotary table with integrated RESOLUTE absolute rotary encoders and Panasonic serial communication protocols for direct interfacing with Panasonic drives and controllers.


Open quotation mark

Although machine tool environments are generally contaminated with metal swarf, oil and coolant, enclosing an open encoder within the motor eliminates any related problems.

Moreover, RESOLUTE's high level of ingress protection (IP64) provides further assurance.

Industrial Technology Research Institute (Taiwan) Close quotation mark








Recommended solutions

Image

Breakthrough in multi-axis rotary table design

Taiwan's Industrial Technology Research Institute (ITRI) has addressed the market trend by developing an advanced dual-axis rotary table with integrated RESOLUTE™ absolute rotary encoders and Panasonic serial communication protocols for direct interfacing with Panasonic drives and controllers.


Open quotation mark

Although machine tool environments are generally contaminated with metal swarf, oil and coolant, enclosing an open encoder within the motor eliminates any related problems.

Industrial Technology Research Institute (Taiwan) Close quotation mark




Image

Sweet spot between cost control and technology advancement

SOLPOWER is a Taiwanese manufacturer of direct-drive rotary tables, integrated spindle motors and linear motors. Effective cost control is key to success in Taiwan’s machine tool industry. RESOLUTE™ absolute  encoders offer advanced features that support the company’s cost-efficiency strategy.


Open quotation mark

We developed the most cost-effective rotary table possible, which means that cost must be strictly controlled from design, parts procurement to production.

Renishaw as a major supplier is an important part of our cost-efficiency strategy.

SOLPOWER (Taiwan) Close quotation mark




Recommended encoder solutions

Machine tools

For machine tools

Paint Point #1

Image

Paint Point #1

Image

Paint Point #1

Image

Paint Point #2

Image

Paint Point #2

Image

Paint Point #2

Image

Paint Point #3

Image

Paint Point #3

Image

Paint Point #3

Image

RESOLUTE™ true-absolute encoder 

The true-absolute encoder with a high-speed fine-resolution position measurement system. Position is acquired immediately on start-up without requiring any motion, offering smooth velocity control and dependable positional stability. Available with linear and rotary scales with a variety of serial interfaces.

✔ High speed

✔ Excellent dirt immunity

✔ Low SDE

✔ Low jitter

Image
Image

FORTiS™ enclosed linear encoder

The next-generation enclosed absolute encoder is built for use in harsh environments, which delivers high performance and significant benefits over conventional systems with an exceptionally robust enclosed design.

✔ Industry-proven position measurement

✔ Superior sealing against dust and coolant

✔ Easy installation with wide mounting tolerances

✔ Non contact design 

SpinCo™ incremental magnetic encoder

Designed for use as primary position and speed feedback sensor for machine tool spindles, the SpinCo™ encoder system consists of two key elements: a readhead and a magnetic ring.

✔ High speed: up to 55,000 rpm

✔ IP67 protection

✔ Signal stability

✔ Small readhead size

Image
Image

LA12 absolute magnetic encoder

Designed for motion control applications as a position and velocity control loop feedback element. LA12’s readhead is sealed to IP67 providing reliable operation with resolutions up to 0.244 µm and supports Mitsubishi, Yaskawa and Fanuc serial communication.

✔ W

✔ D

✔ H

✔ R

AM8192B rotary magnetic encoder IC

Integrates proven filtering optics and interpolation technology into a super-compact, analogue or digital incremental open optical encoder, with wide installation tolerances and built-in calibration functions.

✔ Wide installation tolerances

✔ Dirt immunity

✔ High performance

✔ Robust

Image
Image

OnAxis™ encoder modules

Integrates proven filtering optics and interpolation technology into a super-compact, analogue or digital incremental open optical encoder, with wide installation tolerances and built-in calibration functions.

✔ Wide installation tolerances

✔ Dirt immunity

✔ High performance

✔ Robust

Speak to out manufacturing consultants

Looking for a deeper dive into success stories?


XK10 Used and Trusted

Seeking a tailored encoder solution?


Tell us your requirements and our application engineers will work with you to find the right solution.


Encoder custom solution.png

Learn how much manufacturers are benefitting from using XK10

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Vestibulum consequat mauris eu ullamcorper convallis. Phasellus accumsan, massa in ultrices eleifend, orci nibh commodo nisl, sed sollicitudin arcu urna sit amet enim. Mauris ante turpis, imperdiet eget interdum ac, eleifend volutpat lacus. Integer id nisi cursus, suscipit dui at, auctor ipsum. Suspendisse pulvinar aliquam sapien, id placerat sem tristique vel.

Video #1

Video #2

Video #3

Case Studies

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Vestibulum consequat mauris eu ullamcorper convallis. Phasellus accumsan, massa in ultrices eleifend, orci nibh commodo nisl, sed sollicitudin arcu urna sit amet enim. Mauris ante turpis, imperdiet eget interdum ac, eleifend volutpat lacus. Integer id nisi cursus, suscipit dui at, auctor ipsum. Suspendisse pulvinar aliquam sapien, id placerat sem tristique vel.

Image

Video #1

Image

Video #2

Image

Video #3

Image

Video #4

Image

Video #5

Image

Video #6

loading