Precision stages – achieving precision in the industrial landscape

Precision stages, also known as precision motion stages or motion platforms, are devices used for precise positioning and movement of objects or equipment in various industrial and scientific applications.

The vital role of encoders in precision motion stages


Renishaw's optical and magnetic encoder products.jpg

The global demand for semiconductor manufacturing equipment continues to surge, driven by rapid advancements in artificial intelligence (AI), 5G broadband, and the Internet of Things (IoT). As a result, equipment manufacturers are under pressure to deliver high-precision, high-throughput motion control systems that meet the exacting standards of modern electronics production.


Key semiconductors process equipment includes:
  • Dual wafer stages for photolithography
  • Wafer bonding and laser annealing systems
  • Equipment front-end modules (EFEMs)
XY_stage_440x240.jpg


Position sensing with high-resolution encoders


Precision encoders are integrated into the moving components of the precision stage. These encoders accurately measure the linear or angular displacement of the stage.

Encoders convert the physical motion into electrical signals that can be processed and used for control purposes.

Renishaw_encoder_on_stage.gif
XY_stage.jpg
Encoders within precision stages track linear and angular movement.


The VIONiC™ incremental optical encoder features features intelligent interpolation technology, delivering exceptional repeatability and high-resolution feedback down to 2.5 nm. This makes it ideal for demanding semiconductor applications such as:
  • Wire bonding
  • Mask alignment
  • Die placement



Closed-loop control for reliable motion feedback


Precision stages typically operate within a closed-loop control system, where the encoder provides continuous feedback on the stage’s position. The controller compares the actual and target positions, adjusting movement to maintain accuracy.

This dynamic feedback loop ensures:
  • Precise wafer and mask alignment
  • Reduced positioning errors
  • Enhanced throughput and process stability
Motion_stage_440x240.jpg


High accuracy for critical semiconductor tasks


In manufacturing environments where sub-micron tolerances are essential, high-performance encoders play a pivotal role in enabling accurate and repeatable motion control.

Renishaw encoders support precision stages in tasks such as
:
  • Photolithography - where overlay precision directly impacts yield
  • Optics testing - which demands stable and repeatable alignment
  • Nanotechnology research - requiring sub-micron control across multiple axes

Encoder - wire bonding semiconductor.jpg
High-precision encoders are widely used in the semiconductor IC chip manufacturing process, including in the back-end packaging process, specifically in semiconductor wire bonding operations, also known as wire joining or lead bonding.


➤ Why choose Renishaw’s VIONiC™ encoder for precision stages?


The VIONiC™ incremental optical encoder combines Renishaw’s market-leading optical technology with an intelligent interpolation chip to deliver:
  • Resolution down to 2.5 nm for ultra-fine motion control
  • Exceptional repeatability for consistent performance
  • Compact design for space-constrained semiconductor equipment

These capabilities make VIONiC™ an ideal choice for high-speed, high-accuracy applications, including wire bonding and die placement, wafer inspection and alignment, and multi-axis synchronisation in packaging platforms.


Motion profiling for controlled movement


Precision encoders deliver accurate feedback on speed and acceleration, enabling semiconductor equipment to execute motion profiles with exceptional control. 

Silicon Wafer during Photolithography Process.gifLithography process that allows to create complex patterns on a wafer during semiconductor and computer chip manufacturing.
This motion data supports:

  • Smooth starts and stops, protecting delicate workpieces and tooling
  • Controlled transitions between process steps, enhancing throughput and consistency
  • Reduced mechanical wear and vibration, which extends equipment life and minimises downtime


In semiconductor lithography and wafer handling systems, this high level of motion control ensures repeatable positioning, minimal overshoot, and stable process execution - even at high speeds.


Multi-axis synchronisation with absolute feedback


Semiconductor platforms often require precise coordination across multiple axes - especially in XY and XYZ stages used for mask alignment, die placement, and inspection.

Precision encoders maintain accurate alignment and synchronisation across all axes, even during start-up or after power loss.

➤ Why choose Renishaw’s RESOLUTE™ encoder for precision stages?


RESOLUTE™ absolute encoder delivers instant position feedback and low sub-divisional error (SDE ±40 nm), enabling stable motion control and precise synchronisation across multiple axes.

These capabilities are critical for semiconductor applications such as photolithography and die bonding, where overlay accuracy and repeatable positioning are essential.

Encoder for precision stages.jpg
In an XY stage, encoders are used for each axis to uphold accurate alignment and synchronisation among the axes.

Not sure which one suits you?



What to consider when selecting encoder systems for precision stages?


The table below outlines the key factors typically evaluated when choosing an encoder system for precision stages. These factors include encoder performance, environment conditions, installation requirements, and other relevant considerations.

Precision stages

Performance

✔ Scale accuracy
✔ Scale linearity
✔ Resolution
✔ Sub-divisional error
✔ Axes lengths
✔ Scale CTE
✔ Repeatability
✔ Jitter
✔ Speed
✔ Controller input frequency
✔ Cable flex life
✔ Cable flex radius


Environment

✔ Temperature
✔ Humidity
✔ Vibration
✔ Cleanliness (particle, fluid)
✔ Vacuum / exposure to X-ray radiation / lighting
✔ Electromagnetic compatibility (EMC)

Installation

✔ Size and form factor
✔ Ride height tolerance
✔ Yaw / pitch / roll
✔ Connectors
✔ Cable extension
✔ Readhead travel orientation
✔ Top or side mount
✔ Ease of error diagnosis
✔ Substrate type
✔ Mounting method - adhesive / track / end fixing /epoxy or screw mounted
✔ Reference datum
✔ Limits


Others

✔ Analogue / digital
✔ Interpolation clock frequency
✔ Alarm type
✔ Reference limit
✔ Protocol


Got questions? Let us help you choose!

Encoder success stories: Precision stages

Heading 1

Lorem Ipsum is simply dummy text of the printing and typesetting industry. Lorem Ipsum has been the industry's standard dummy text ever since the 1500s, when an unknown printer took a galley of type and scrambled it to make a type specimen book.

Form Heading

Semiconductor - the world’s No.1 manufacturer

ASM Pacific Technology Ltd (ASMPT) is the world's largest supplier of wafer assembly and packaging equipment for the semiconductor industry. ASMPT's equipment is renowned for high precision and high stability.

Consequently, it demands reliable and high quality positioning systems, including ‘dirt immunity' capability. Patented optical schemes are built into every Renishaw encoders’ readhead to withstand a variety of contaminants, such as grease, dust, particles and scratches.


Open quotation mark

The positive feedback from our customers has proven that Renishaw's encoders have excellent dirt immunity and can run reliably with little or no maintenance.

ASM Pacific Technology Ltd (Global) Close quotation mark


A wide variety of Renishaw encoders is employed in various ASMPT machines, including the TONiC™ incremental optical series, the RESOLUTE™ absolute optical encoders , and LM10 magnetic encoders.

Image

Renishaw encoders are employed in various ASMPT machines:

•   AB559 series wedge bonders: designed with a large aluminium bonding area of 8 inches x 4 inches and speeds to 4.1 wires/sec
•   High speed MCM12 die bonders: a fully automatic multiple die, SMD, and flip chip bonding system, up to 14 types of picking tools and 12 inch wafer handling capability
•   SMD and flip-chip bonders: with up to 300 mm wafer handling capacity
•   UV Cured Die bonders: used in image sensor applications with resolutions to 50 nm and speeds to 3.5 m/s in operating temperatures as high as 300 ºC



Semiconductor - competitive edge in the marketplace


Beijing U-Precision Tech Co., Ltd. (U-Precision) is a leading manufacturer of equipment for high-precision industrial processes. Its advanced semiconductor equipment and motion stages use mostly TONiC™ optical encoder systems with steel tape scales.

Renishaw's TONiC™ incremental encoders have been specially designed for semiconductor applications and give OEM manufacturers, such as U-Precision, a competitive edge in the marketplace.


Open quotation mark

Optical encoders are one of the most important components of stages and process machinery, so we went through an exhaustive evaluation process before choosing Renishaw, and we continue to use their products to this day.

Beijing U-Precision Tech Co., Ltd. (China)Close quotation mark



Precision motion platforms - cost-effective and high performance


Renishaw's TONiC™ UHV optical encoders are specially designed for use in high and ultra-high vacuum enclosures and meet the strict requirements of FPD and semiconductor process equipment.

VAD Instrument manufactures a wide range of precision motion platforms for use in a vacuum environment for semiconductor, FPD and electronics applications. The company selected TONiC™ UHV encoder and RLE fibre optic laser encoder for its latest range of vacuum compatible platforms.


Open quotation mark

Renishaw's encoder products have a good reputation in the marketplace; the TONiC™ encoder series is often seen in applications with high-performance equipment and has been widely recognized by the industry.

VAD Instrument (South Korea) Close quotation mark

VAD Vacuum stage 480x300.jpgVacuum stage for semiconductor process application.



DD motors - win orders with OEM innovation


JUSTEK Inc. is a leading motion control component manufacturer in Korea. It designs and builds linear motors, direct-drive rotary (DDR) motors, motion stages and conveyors. Renishaw's family of ATOM™ miniature encoder solutions has been chosen by JUSTEK for its DD motors and motion stages.

“The miniature design of the ATOM™ readhead is ideal for our DD motors as space inside the motors is inherently limited. We tested ATOM™ repeatedly and found that it has advantages in terms of reliability, system volume and performance.” JUSTEK's product manager explained.


Encoder for stages - Justek.pngDDR motor (JTR30 series) manufactured by JUSTEK.


Open quotation mark

Renishaw is highly regarded in the metrology industry and has been involved with our products over many years.

JUSTEK Inc. (South Korea) Close quotation mark


Renishaw's ATOM™ optical encoder has a readhead measuring just 7.3 x 20.5 x 12.7 mm. It is one of only a handful of integrated miniaturised optical encoders available on the market and features leading-edge signal stability, dirt immunity and reliability.

Renishaw optical encoders adopted by JUSTEK including:

•  ATOM™ miniature encoder series for DD motors and motion stages.
•  TONiC™ incremental encoder series for OLED panel inspection equipment.
•  RESOLUTE™ absolute encoder series for OLED panel inkjet printing equipment.

Image

Precision motion platforms -

cost-effective and high performance

---

Image



Recommended encoder solutions

Precision stages

For electric vehicles (EVs)

Paint Point #1

Image

Paint Point #1

Image

Paint Point #1

Image

Paint Point #2

Image

Paint Point #2

Image

Paint Point #2

Image

Paint Point #3

Image

Paint Point #3

Image

Paint Point #3

Image

VIONiC™ digital incremental encoder

High performance digital optical encoder designed with super compact readhead, suitable for highly-dynamic precision motion systems.

✔ Superior metrology

✔ High speed operation with fine resolution

✔ Ultra-low sub-divisional error (SDE)

✔ Cost benefit


Image
Image

TONiC™ incremental encoder

A high performance optical encoder designed with super compact readhead, suitable for highly-dynamic precision motion systems.

✔ (Very) low jitter

✔ Fine resolutions down to 1 nm

✔ Cost benefit


RESOLUTE™ true-absolute encoder 

The true-absolute encoder with a high-speed fine-resolution position measurement system. Position is acquired immediately on start-up without requiring any motion, offering smooth velocity control and dependable positional stability. Available with linear and rotary scales with a variety of serial interfaces.

✔ High speed

✔ Excellent dirt Immunity

✔ Low SDE

✔ Low jitter

Image
Image

ATOM™ miniature optical encoder

The miniature optical incremental linear and rotary encoder system offers innovative design combining miniaturisation with leading-edge signal stability, dirt immunity and reliability.

✔ Miniature

✔ Advanced signal stability

✔ Dirt immunity

✔ Reliability


AtomDX-size.png

QUANTiC™ incremental encoder

Integrates proven filtering optics and interpolation technology into a super-compact, analogue or digital incremental open optical encoder, with wide installation tolerances and built-in calibration functions.

✔ Wide installation tolerances

✔ Dirt immunity

✔ High performance

✔ Robust

Image
Image

LM10 incremental magnetic encoder

The LM10 is a contactless high-speed magnetic encoder designed for linear or rotary motion sensing in harsh environments. The LM10 features a compact sealed readhead that rides at up to 1.0 mm from the self-adhesive magnetic scale or ring.

✔ Stick-on reference mark

✔ High speed operation

✔ Excellent dirt Immunity to IP68

✔ Axis lengths of up to 100 m

✔ High reliability

Speak to out manufacturing consultants

Looking for a deeper dive into success stories?


XK10 Used and Trusted

Seeking a tailored encoder solution?


Tell us your requirements and our application engineers will work with you to find the right solution.


Encoder custom solution.png

Learn how much manufacturers are benefitting from using XK10

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Vestibulum consequat mauris eu ullamcorper convallis. Phasellus accumsan, massa in ultrices eleifend, orci nibh commodo nisl, sed sollicitudin arcu urna sit amet enim. Mauris ante turpis, imperdiet eget interdum ac, eleifend volutpat lacus. Integer id nisi cursus, suscipit dui at, auctor ipsum. Suspendisse pulvinar aliquam sapien, id placerat sem tristique vel.

Video #1

Video #2

Video #3

Case Studies

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Vestibulum consequat mauris eu ullamcorper convallis. Phasellus accumsan, massa in ultrices eleifend, orci nibh commodo nisl, sed sollicitudin arcu urna sit amet enim. Mauris ante turpis, imperdiet eget interdum ac, eleifend volutpat lacus. Integer id nisi cursus, suscipit dui at, auctor ipsum. Suspendisse pulvinar aliquam sapien, id placerat sem tristique vel.

Image

Video #1

Image

Video #2

Image

Video #3

Image

Video #4

Image

Video #5

Image

Video #6

loading